Issue
Is Vista OPC server supported on a 64-bit operating system?
Environment
- TAC Vista 5.1.6
- TAC Vista OPC server 1.1.6
- 64-bit operating system
Cause
TAC Vista OPC server 1.1.6 is not officially supported on a 64-bit system
Resolution
TAC Vista OPC server 1.1.6 is not officially supported on a 64-bit system, but it has been tested on a limited run and no problems have occurred. It is always better to stick with recommended and supported hardware, but in this exception, it may be okay.