Issue
In TAC Webstation is it possible to not go to the login page when logging out from TAC Webstation?
If using single sign on no login is needed for the customer so when clicking the logout button he like to go the home page and not the login page for Webstation.
Environment
TAC Vista 5.1.6
TAC Vista Webstation 5.1.6
Cause
No this is not possible, it is hardcoded in the program to go to the login page when logout from TAC Webstation.
Resolution
No this is not possible, it is hardcoded in the program to go to the login page when logout from TAC Webstation.