Issue
Cannot upgrade the OS of i2 controller with the error message of "Controller Type Mismatch" .
Environment
NetController (bCX9640)
InfinetController (i2xxx)
Cause
When upgrading the i2 controller to the latest version AND the version of NetController (bCX9640) is couple of versions older than the i2 controllers new version.
Resolution
Upgrade the NetController to the latest version of OS first, reload the NetController, reload the i2 controller and then upgrade the i2 controller to the latest version.