Issue
Is there a native solution in Continuum to totalize the hours of presence of a person in an area? Or must I do a PE program for each personnel which will calculate the time between the arrival time and the leaving time?
Environment
Time and Attendance
CyberStation
ACX and/or AC-1 family of controllers
Cause
Is there a native solution in Continuum to totalize the hours of presence of a person in an area? Or must I do a PE program for each personnel which will calculate the time between the arrival time and the leaving time?
Resolution
There is no native solution in Continuum to totalize the hours a person has spent in a given area. It will require PE programming and entry and exit readers.
The Security COE has a Continuum add-on called TimeTracker that may work for some applications. Learn more about Continuum Time Tracker.