Issue
What is the maximum recommended wiring length on an ADI or remote I/O wiring segment?
Environment
MNB-1000, MNB-1000-15
Cause
What is the maximum recommended wiring length on an ADI or remote I/O wiring segment?
Resolution
The maximum recommended length of an ADI or remote I/O wiring segment is 4000 ft (1200 m), using the cables listed for “76,800 or Less” baud rate.
Information on approved cable types and additional information cane be found in chapter 1 of the “I/A Series MicroNet BACnet Wiring, Networking, and Best Practices Guide” (F-27360-5).