Issue
Application is to open a door with a PIN Number instead of a card read.
Environment
I/NET Seven versions 2.4X and above.
Cause
The Customer is wanting to use a "PIN Only" function at a Pin Pad reader to gain access thru a door
Resolution
The following document describes the procedure controlling a door using the Door Code Feature.