Issue
Any objects created get placed in the folder
Environment
Continuum
Windows XP
Windows Vista
Windows 7
Windows Server 2003
Windows Server 2008
Cause
Selecting the checkbox for put object in folder and specifying a folder causing all objects to default to this folder.
Resolution
By default, this checkbox isn't selected. To go back to normal functionality, uncheck the checkbox to 'put object in folder' and remove the specified folder.
When this mistake is made, not one single point can be named the same in similar controllers that are under that NetController or BCX.
This can affect drag and drop also.