Issue
Door needs to be set to SiteMode+CardMode for weekdays and SiteMode+CardMode+PinMode for weekends.
Product Line
Andover Continuum
Environment
- NetController (CX9900 , CX9940 , CX9702 , ACCX5740 , ACX5730)
- InfinetController (ACX780, ACX781)
Cause
Customers want to have a PE program that changes the door mode to be more secured for the weekend according the building schedule.
Resolution
In the PE program ;
Set DoorName\EntryNormMode = 3 ' Set the door mode to SiteMode+CardMode for weekdays
Set DoorName\EntryNormMode = 11 ' Set the door mode to SiteMode+CardMode+PinMode for weekends.
The values for the different modes are:
- 1 = SiteMode
- 2 = CardMode
- 4 = GeneralMode
- 8 = PINMode
- 16 = ScheduleMode
The individual values are added together to obtain the desired mode. As seen above, setting the mode to 3 makes the door validate site + card.
It is recommended that both the normal and nocomm modes be set (EntryNormMode, EntryNoCommMode)
For a dual reader door, use the corresponding ExitNormMode and ExitNoCommMode.