Issue
Can additional resources be added to an ENC-SW (Soft JACE) to increase the resources over the 30,000 KRu (30 Million) limit?
Environment
I/A Series G3, ENC-SW
Cause
Can additional resources be added to an ENC-SW (Soft JACE) to increase the resources over the 30,000 KRu (30 Million) limit?
Resolution
The I/A Series G3 Soft JACE can be initially purchased to support 10,000 KRu (10 Million) resources. Additional resources can be added to the 10,000 KRu (10 Million) version to increase the total to 30,000 KRu (30 Million). The maximum number of licensed resources per ENC-SW (Soft JACE) is 30,000 KRu (30 Million).
ENC-SW-1M >> Support for 10,000 KRu (10 Million) resources
ENC-SW-2MU >> Upgrade ENC-SW-1M to increase total to 30,000 KRu (30 Million) resources