Issue
- Values are not updating in a specific TGML graphic in webstation.
- Red x on all values in a TGML graphic, other graphics working fine.
- Crossed out values in TGML graphic.
- String value (text) with " in the text not displaying
Product Line
TAC Vista
Environment
- TAC Vista 5.1.6
- TAC Webstation 5.1.6
Cause
If there is a string value (text value) in the graphic with the a double quote quotation mark (") in the text, all signals stop updating on that graphic.
Resolution
Make sure there are no " in any string on the graphic.