Issue
A new MicroNet VAV controller has been installed under a MicroNet Microsmart Integrator (MN-MSI). How is real-time data obtained from and how are commands sent to the new VAV controller?
Environment
MN-FLO3x
MN-MSI
DMS-35, -350A, -3500
Cause
The MN-MSI is an obsolete product and no documentation is available for it.
Resolution
To integrate the new MicroNet VAV controller with a MN-MSI, create a Mode Control point Type 26 in the MN-MSI using the programming tool called DMS Operator Interface (also called PS-OPRIF or just OPRIF).
Use this file to learn and program the Type 26 Mode Control point. It is a complete chapter from the MN-MSI documentation.