Issue
Password, Passcode for a UNC532 or a UNC632 Keyboard.
Environment
Sigma, BAS, UNC532 Keyboard, UNC632 Keyboard.
Cause
What is the password passcode for a UNC532 Keyboard or a UNC632 Keyboard.
Resolution
The default passcodes are:
2001
1066
1482
0338
8420
Keypads that were used in BAS are now replaced by PDA's.
Keyboards can only interrogate the controller they are fitted to and are can only be fitted to UNC532 or UNC632 controllers.