How to modify, save, and install Microsmart UDPs in UltiVist

Issue

How to modify, save, and install Microsmart UDPs in UltiVist

Product Line

TAC I/A Series

Environment

UltiVist (any version)

Cause

n/a

Resolution

Procedure:

  1. Highlight the Microsmart controller.
  2. Click on the Functions drop-down menu and select UDP Status.
  3. Double-click the UDP number of choice.  Click overtop the UDP descriptor or UDP status portion of the line.
  4. Select PROGRAM from the pop-up window.
  5. A Watson Works Editor (EPM) appears with a blank screen.
  6. Press Enter and begin adding the program code.
  7. When complete click the Save button in the toolbar and exit the window.  Alternatively, click on the File drop-down menu and select Save and quit.  NOTE:  Do not do a "Save As" and do not change the name of the file.  The filename at the top will appear as D:\FI\E4000000 or similar.  Do not modify it.
  8. Back on the UDP Status screen, double-click the just-programmed UDP.  Select INSTALL from the pop-up window.
  9. When the INSTALL completes, double-click it again to ENABLE it.