What voltages will a BAS 2000/BAS2800/BAS2800+ outstation operate under.

Issue

The need to know What voltages will a BAS 2000/BAS2800/BAS2800+ outstation operate under.

Product Line

Other

Environment

  • BAS2000
  • BAS2800
  • BAS2800+
  • Power Voltage Input
     

Cause

The need to know What voltages will a BAS 2000, BAS 2800, BAS 2800+ outstation operate under.

Resolution

For a BAS 2000/BAS2800/BAS2800+ outstation the specification for the power supply is shown as: -

Power Supply: 220V (-15%) to 240V (+10%), 50Hz (-10%) to 60Hz (+10%)
Consumption: 0.16A max @ 240V 50Hz
Heat Dissipation: 25W max, 10W typical