What voltages will a Sigma controller operate under.

Issue

The need to know what voltages will a Sigma controller operates under.

Product Line

Satchwell Sigma

Environment

Sigma Power Voltage Input

Cause

The need to know what voltages will a Sigma controller operates under.

Resolution

For Sigma controller the specification for the power supply is shown as:

Supply voltage. . . . . . . . . . . . . . . . . . . . .230Vac ±10%.
Supply frequency. . . . . . . . . . . . . . . . . . .50/60Hz ±10%
Power consumption. . . . . . . . . . . . . . . . .25VA maximum