Issue
I/A Series G3 SMS Driver Part Number
Product Line
TAC I/A Series
Environment
I/A Series G3
Cause
The SMS (Simple Message Service) driver is used for sending text messages to mobile / cellular phones. The SMS driver allows retransmitting alarm information and sending general text messages.
The I/A Series G3 SMS driver is not listed in the datasheets for the Enterprise Network Server or Enterprise Network Controllers.
Resolution
ENC-DRV-SMS
License an ENC-520, JACE 6 or JACE 7 to enable SMS alarms to be sent to any mobile phone via a GSM/GPRS modem connected to the RS-232 serial port
* The SMS Driver is no longer available in the Enterprise Network Server and Soft JACE. There is a technical issue and the driver has been removed from use on Windows based platforms.
If the driver is required for use in the ENC or Soft JACE, contact Schneider Electric Product Management via your local Schneider Electric sales office.
If the driver is required for use in the ENC or Soft JACE, contact Schneider Electric Product Management via your local Schneider Electric sales office.
ENC-DRV-SMS
License an ENC-520, JACE 6 or JACE 7 to enable SMS alarms to be sent to any mobile phone via a GSM/GPRS modem connected to the RS-232 serial port