Issue
A Niagara R2 installation is being upgraded to the current revision. What's the part number for ordering an upgraded license file?
Environment
Niagara R2
Cause
Installation is being upgraded from 2.301.431 to the current revision
Resolution
IA-LIC-23G
Upgrades the license file to the current revision
IA-LIC-CHG
Modifies other parameters in the license file like the projectId, orgId, hostId, etc....
Both part numbers apply to an Enterprise Server license and to an UNC license.
The list price for both of these part numbers is available on iPortal.