Issue
Unable to get I/NET to install on Military Bases.
Environment
Windows 7 and Windows Vista OS with I/NET Seven versions 2.40 and above.
Cause
The version of software that is being used by the military does not allow the password scheme to create the necessary permissions for correct functionality.
Resolution
- Remove I/NET from the PC.
- Reconfigure the PC with the original version of Windows and or Vista
- Load I/NET on this version.
- Upgrade PC to Windows 7 Gold or Windows Vista Gold
- Once completed then restart I/NET again.