Issue
Does the ECH-75010R (Echelon U-10 USB Adapter) come with the interface cable?
Data sheet does not specify this information.
Environment
Echelon U-10 USB Adapter
Cause
Data sheet does not specify what interface cable, if any is included with the U-10 adapter.
Resolution
The Echelon U-10 LON Network adapter does not come with an interface cable.
As documented in the Echelon data sheet, the adapter only comes with a USB extension cable.
To use this adapter with the I/A Series LON controllers, the WPIA-CBL-1 is required.