How to change the name of a 527 Link or DLA site

Issue

How to change the name of a 527 Link or DLA site

Product Line

TAC I/NET

Environment

I/NET Seven

XBuilder

Xenta 527

Cause

In some versions of I/NET changing the name of a Link name through the I/NET Configuration tool will not work on a Xenta 527.

Also, You cannot configure the Name of Link through Xbuilder, this must be done as show below.

Resolution

Before you begin, follow the instructions on Lessons Learned 6372 If this fails, or you are performing an initial configuration via XBuilder, use the process below.

  1. Connect to the Xenta 527 via a web browser
  2. Expand the Configuration folder
  3. Expand the Network folder
  4. Click on TCP/IP
  5. Change the Host Name to the desired link name.