Issue
- Links in TGML graphics in Webstation do not work.
- A page can not be opened error message is shown.
- No Java is installed, TGML viewer mode in Websettings is set to Autodetect and "Optimized TGML loading" is set to On.
Environment
- Vista Webstation 5.1.6
- TGML Graphics
Cause
For some reason the links do not work when no Java is installed, TGML viewer mode in Websettings is set to Autodetect and "Optimized TGML loading" is set to On.
Resolution
In Vista Websettings change "Optimized TGML loading" to Off.