Quick time movie to indicate CPU light modes for controllers

Issue

Troubleshooting controllers can be aided by observing the CPU light

Product Line

Andover Continuum

Environment

Continuum controllers

Cause

A quick time movie was created to show the differences between bootloader, normal and error

Resolution

This will not tell you specifically what mode the controller is in, but it can offered to try to help to determine the mode.

The speed of the CPU light on some of the controllers may vary, but this gives a general idea.

Click to download the quick time movie