Issue
Certain versions of Cyberstation use a different number of indexes by default.
Environment
Continuum
Microsoft SQL Server
Cause
Some IT departments like to know how many indexes are used in their application databases
Resolution
1. The amount of indexes used is based on Cyberstation version
To see the number of indexes and additional information use Enterprise Management Studio to run a query on the Continuumdb
select * from sys.indexes
2. Additional indexes can be created by DBAs for optimization and performance reasons, but these are not the defaults.