Issue
A university customer has two personnel "types" - faculty/staff and student. They would like to link a different Personnel Manager profile to each type of personnel so that when the record is edited it opens using that profile. Can this be done?
Environment
CyberStation
Personnel Manager
Cause
A university customer has two personnel "types" - faculty/staff and student. They would like to link a different Personnel Manager profile to each type of personnel so that when the record is edited it opens using that profile. Can this be done?
Resolution
Unfortunately, this is not a feature in the current (v1.93) or older CyberStation versions.
You can open the Personnel Manager and then switch to a different profile and enter the personnel data, but that profile is not linked to the saved record. So, subsequent editing of the record will open in the default (current) profile.