External alarms, trends and time schedules for programmable Xenta controllers in an LNS system

Issue

Is there any need to set up external alarms, trends or Time schedules for Programmable Xenta controllers if I use a LNS system?

Product Line

TAC Vista

Environment

TAC Vista LNS

TAC Xenta 301, Xenta 302,

TAC Xenta 401

TAC Xenta 281, Xenta 282, Xenta 283

Cause

Differences in classic and LNS scenario

Resolution

No there are no need to set up any external alarms, the proprietary communication still works.