What is the part number for the battery in a Network 8000 GCM?

Issue

What is the part number for the battery in a Network 8000 GCM?

Product Line

TAC I/A Series

Environment

Network 8000 GCM-84000 series, GCM-86000 series, LNC-100, SIM-CCN, SIM-MTECH, SIM-TRANE, and SIM-YORK.

Network 8000 LCMs.

Cause

Need to replace a discharged  battery in a GCM or an LCM.

Resolution

The part number for the replacement battery is E17-129.
NOTE:  The E17-131 is a functional replacement for the E17-129 which is now obsolete.  The E17-131 can be found on iPortal

 

For a GCM-86000 series, LNC-100, SIM-CCN, SIM-MTECH, SIM-TRANE, and SIM-YORK, replace the battery according to
F-25895, GCM-861X0 Series Global Control Module Installation Instructions, "Battery", "To Enable Battery", "To Replace Battery", and "Checkout" sections.

For a GCM-84000 series or an LCM, replace the battery according to F-23116, "LCM / GCM Battery Installation Instructions".