Sigma - Diagnostic LED's on the UNC 532 / 632 and the UNC 496 / 596 / 696 / 796 controllers and DNN / DNN3.

Issue

Understanding the meaning of the Diagnostic LED's located on UNC devices.

Product Line

Satchwell Sigma

Environment

Sigma

Devices

Controllers

UNC

DNN

DNN3

496

532

596

632

696

796

Cause

The Diagnostic LED's provide the user with a clear understanding of the controllers present state.

Resolution

The LED chart below provides a clear understanding of the controller state, and allows an easy diagnostics.