Continuum Compatibility Matrix supersedes compatibility information on other documents.

Issue

The CyberStation installation guide states that the Continuum DB Server can be run on a Windows 7 PC while the Continuum Compatibility Matrix does not. 

Which document is correct? 

Product Line

Andover Continuum

Environment

CyberStation

WebClient

ContinuumDB Server

Cause

Because their are a variety of documents that describe system requirements for various Continuum products, it is unfeasible to update system requirement information in each document every time a change occurs.

For this reason the Continuum Compatibility Matrix should be used as the ultimate word on Continuum products and controllers and the software and firmware that support them.

Resolution

The Continuum Compatibility Matrix is the ultimate authority when it comes to hardware/software/firmware compatibility.