AC1/AC1A does not have alternate LED pattern

Issue

Replaced an AC1Plus with an AC1 and the reader pattern is incorrect

Product Line

Andover Continuum

Environment

Continuum

AC1

AC1A

Cause

The AC1/AC1A module only has 1 LED pattern which is Alternate LED pattern, there is no way to alter this. 

 

See http://buildingskb.schneider-electric.com/view.php?AID=2860 for description of LED patterns

Resolution

If a different LED pattern is required by the site then use an AC1 plus or an ACX57xx which gives the ability to use an alternate LED pattern. See Lessons Learned Article #2860 for configuration.