Issue
Personnel distributions failing due to illegal card numbers configured in personnel objects.
Environment
- CyberStation
- Personnel Objects
Cause
Each card type has restrictions as to what site codes can be used and the maximum card number that can be used.
Resolution
The following is a summary of card types and the site codes and card numbers that are available to each.
Card Format | Site Code | Card Number |
---|---|---|
Wiegand26 | 0 – 255 (8-bit) | 0 – 65535 (16-bit) |
Infinity_37 | 0 – 4095 (12-bit) | 0 – 524287 (19-bit) |
HIDCorp1000_35 | 0 – 4095 (12-bit) | 0 – 1048575 (20-bit) |
CustomWiegand | 0 - 65535 (16-bit) | 0 – 4294967295 (32-bit) |
Note: Site codes of 0 cannot be entered through the old style Personnel Editor, use Personnel Manager or set attributes through a list view.