SNVT (Standard Network Variable Types) on Function Block Program

Issue

 SNVT on FB Program 

Product Line

SmartStruxure Solution

Environment

StruxureWare Building Operation site

Cause

When you create a SNVT in a functional block and you copy it for a new one and after you rename the copied SNVT, When you commissioning the local node with a LNS tool the node keeps the first name.

Resolution

The SNVT (Standard Network Variable Types) copy issue exists. Where it is happening is that the XIF file in the device is not getting updated when the signal name changes. An LNS management tool will upload this XIF file and use it to see the values. This has been reported as bug in software and will be resolved in an upcoming release.