CSMC 3805 Codes, CSMC User Guide.

Issue

CSMC 3805 Codes, CSMC User Guide.

Product Line

Field Devices

Environment

CSMC3805

CSMC

CSMC 3805

Cause

There is a code displayed on the controller screen. What does this mean?

Resolution

The codes display the plant status under certain conditions. They are as follows:

L05 = Return Water Temperature Low Limit.

F = Water Frost Limit (Flow or Return).

L01 = Inside Low Limit (Frost).

H4 = Flow Water High Limit.

A = Alarm (If alarm display is not required set code B61 to 1).

0 to 9 = Optimiser Status (only displayed if code B49 is set to 1).

The User Guide can be downloaded from here.