Issue
What is the acceptable range of tolerance for resistance on a supervisory input.
Environment
- i1 controllers
- i2 controllers
- b3 controllers
- I/O modules
Cause
Doors are being retrofitted, and the resistors that are installed are not 10K ohm and are inaccessible.
Resolution
The tolerance for the resistance on supervisory inputs is +/- 3%.