How can I declare a point to be both an input and an output in a Script program?

Issue

Need to be able to read and write to a point.

Product Line

SmartStruxure Solution

Environment

  • StruxureWare Building Operation Workstation
  • ES
  • AS

Cause

Need to be able to read and write to a point.

Resolution

Declare the point as Output and bind it.

Outputs can be read and written.