Issue
A seven day schedule has been setup in the MNB-1000 using WorkPlace Tech but I don't see any way to set the controller time?
Environment
WorkPlace Tech 5.X, Commissioning tool
Cause
The time and date in the MNB-1000 cannot be defined using WorkPlace Tech.
Resolution
Open the WorkPlace Tech Commissioning tool, locate the desired controller in the Device list and open the Device Properties for that device. On the Device Properties - General tab there is a "Device Clock>>" button used to synchronize the MNB-1000 to the PC's time and date. This is also where the Time Zone is defined for the MNB-1000.