Differences between webclient and Cyberstation

Issue

There are a number of difference between Cyberstation and webclient

Product Line

Andover Continuum

Environment

Webclient

Continuum

Windows XP

Windows Vista

Windows 7

Windows Server 2003

Windows Server 2008

Cause

There are different features and abilities in webclient and Cyberstation and it's necessary to understand those differences.

Resolution

The webclient installation guide has a section in it that describes the main differences. 

As a general rule use Cyberstation to create and administer objects in Continuum and webclient browsers to view those objects.

Click Here - to download an excerpt of the Install guide explaining the differences.

** Graphics are slower through webpinpoint. Higher availability graphics may require a Cyberstation.