V321 (DN65 to DN100), M800, M1500, MV15B, M3000

Issue

The Forta range actuator does not fit onto the V321 Valve.

Product Line

Field Devices

Environment

V321

M800

M1500

MV15B

M3000

Cause

The actuator has a 10mm fitting, the valve (DN65 to DN100 only) spindle has a 8mm stem.

Resolution

On V321 valves size DN65 to DN100 an adaptor piece is supplied with the valve part no. 880-0133-000 to adapt the valve spindle to the actuator drive.

The part no. 880-0133-000 can be ordered separately.