Issue
Is it possible to create a switch, in TGML, which has a popup dialog to confirm the action taken (Yes/No)?
Environment
TGML editor 5.1.X
Vista workstation 5.1.X
Webstation 5.1.X
Cause
A customer wishes to confirm changes before applying them, to avoid setting variables by mistake.
Resolution
In the components library in TGML editor, there is a check box component which has a confirm function. Drag & drop the component onto the workspace and study the code. This can be used as a basis for a switch component.