Issue
V241 / V341 valves do not automatically come complete with connections.
Environment
Valves
V241
V341
Connections
Pipework connections
Cause
The valve body is purchased separately to the connections.
Resolution
When purchasing a V241 / V341 valve it must be remembered that the valve body and the connections have separate specification numbers.
Example to purchase a 32mm V341 valve.
Valve body - 731-4141-000
Connection types available;
Internal thread connection (Standard) - 911-2100-32 (*3)
Soldering type connection (Standard) - 911-2101-32 (*3)
Welded type connection (Standard) - 911-2102-32 (*3)
Note:- you will require the same number of connections as there are ports on the valve.
For the details of the V241 please click HERE.
For the details of the V341 please click HERE.
For the details of the connections please click HERE.