Issue
Which actuator should be used as replacement to a M15 actuator that is mounted on a VTRA Valve?
Environment
VTRA DN65
M15 24V / 12VA 15 Nm 300s / 180°
Cause
Currently used actuator is no longer available.
Resolution
Use EM9/180 (part no 8601110000) together with Linkage kit E/M9-VTRA (part no 8600990000).