Issue
- Xenta server stand alone and Vista at the same time.
- No alarms showing in TAC Vista when Xenta Server is connected.
Environment
TAC Vista
TAC Xenta Server
Cause
If you add a stand alone Xenta Server on a Lon network it will send out heartbeats just like TAC Vista does.
So the affect will be the same as having 2 TAC Vista servers on the same network. But there is a way to turn this off.
In Xbuilder you can turn this off by setting "Alarm Server" to disabled
Resolution
- In Xbuilder click on the LON object
- Under General properties change "Alarm Server" to disabled.
- Download the project.