Issue
Is the DC1100C still available?
Is the DCCOMMS software still available?
Environment
DC1100C
DC1100 C
DCCOMMS
DC COMMS
DC1100
DC1400
DC1000C
DC1000 C
Cause
Is the DC1100C and the DCCOMMS software still available?
Resolution
The DC1100C had the communication module so that the controller could be interrogated remotely. This controller is no longer available. The DCCOMMS software ran in a DOS environment and is also obsolete.
The DC1000C or DC1100C must not be confused with the DC1100 or the DC1400, these are the same controllers but without the communication interface and are still available.