Issue
When changes are made to the BACnet schedule in a third party device, the object editor crashes when the changes are applied.
ACCTrace file shows the following error:
The datatype of a BACnet property value specified in a service parameter does not match the datatype of the property referenced by the specified Property_Identifier.
Environment
CyberStation
Continuum
BACnet
Trane SC Schedule Object
Cause
The object type is not fully support by the third party controller. Consult the devices PICS statement.
Resolution
In some cases third party vendors will implement BACnet object types for internal use while not allowing other vendors to write to these object.
Occasionally it may be possible to write values to some of the objects properties. However, when Continuum tries to write to a value to the unsupported property the object error will crash.