Issue
The AcquiSuite A8812 responds with Error 11: Resource Temporarily Unavailable.
Environment
Niagara G3 / R2
Cause
The AcquiSuite A8812 internal I/O module (Analog and Pulse inputs) uses Modbus address 250. This is not a legal address for a modbus slave device or ID. Valid Niagara addressing is from address 1 to 247 as stated in the Modbus protocol documentation.
Resolution
The Acquisuite Obvius LLC company offers a Flex I/O module that can be addressed between 1-247.