Issue
Vista does not allow the user to edit standard graphics. Attempting to edit a standard object will result in the following error:
Environment
TAC Vista
OGC Graphics
Cause
Vista does not allow the user to edit a standard graphic file within the vista database. A standard graphic is more of a shortcut to the master graphic in the root directory of TAC Vista
Resolution
Only make edits to the master graphic within the root directory of TAC Vista. This change will automatically be changed to all standard graphics associated to it.