Issue
Webpinpoint requires mime types and if a selected option is missing, the object doesn't show in IIS
Environment
Windows 7
Windows Vista
Windows Server 2003
Windows Server 2008
Cause
If all the IIS options in IIS that are specified in the webclient installation guide are not selected then objects for webclient installation will not be available.
Resolution
In Windows Control Panel> Programs and Features> Turn Windows Features On/Off
Make sure that Common HTTP Features> Static Content is checked
If not, check this options and restart the PC