Issue
Launching all graphics on multiple Cybers shows Pinpoint as a white screen
Environment
Continuum
Windows XP
Windows Vista
Windows 7
Windows Server 2003
Windows Server 2008
Cause
The active polling rate may be too high
Resolution
Set the active polling rate to 100 milliseconds
Default is 30