Configuring a Multical 601 meter.

Issue

What is necessary to do in order to change settings in the Kamstrup Multical 601 meter?

Product Line

Field Devices

Environment

Kamstrup Multical 601

Cause

How to change the basic settings in pulse calculations from MWhrs to kWhrs, and also other settings.  

Resolution

Metertool software (part no: MAHWSWTOOL) together with the Optical eye USB hardware (part no: MAOPTICUSB) is required for this type of configuration. For more information, please take a look at MeterTool for Multical 601 presentation.