Issue
Unable to get a point to come up front when it goes in Alarm.
Environment
All versions of I/NET Software.
Cause
Point needs to come upfront when the Alarm is triggered but it is not working.
Resolution
To resolve this issue there are a few steps that needs to be followed to get this working.
- Open the graphic page in the Edit Mode
- Right Click and Select Properties
- In the Page Options, check the boxes for Home Page and Automatic Page Display
- Save the changes and then open it up live again
- Trigger the Alarm to verify that it is coming up front and the page is displayed