Issue redirecting system alarm using Configure alarms in the Vista server

Issue

I have a problem with redirecting a $EE_Mess alarm  using "Configure alarms" in the Vista server. The alarm is not redirected to the new alarm object and therefore not changing the priority.

Product Line

TAC Vista

Environment

Vista server 5.1.6

Cause

$EE_Mess should be redirected to message object in Vista.

A change of state should be redirected to another change of state object in Vista

Resolution

Redirect the $EE_Mess to a message object in Vista and not to a change of state.

Refer to article#7557 for a guide on how to create a system alarm to handle offline alarms